PXA — N9030A/B
This adjustment determines the noise figure of the analyzer down conversion chain and generates several corrections which are stored in memory. The corrections are used to predict the noise that is present at the analyzer input connector.
|
|
Option NF2 generates the adjustment data with an internal alignment that is a manual noise floor characterization. To do this, press System > More > Advanced > Characterize Noise Floor. |
Seven Band/Path combinations are characterized in this adjustment:
Lowband Path, Preamp Off
Lowband Path, Preamp On
Highband Path (Bands 1 – 6), Preselector On, Preamp Off
Highband Path (Bands 1 – 6), Preselector On, Preamp On
Highband Path (Bands 1 – 6), Preselector Off, Preamp Off
Highband Path (Bands 1 – 6), Preselector Off, Preamp On
Highband Path (Bands 1 – 6), Preselector On, Low Noise Path
This adjustment should be performed if the analyzer fails the Effective DANL test or if any component in the RF downconversion chain is changed. This adjustment does rely on the Frequency Response corrections, so this adjustment should be performed after the Frequency Response adjustment.
Click here for troubleshooting.
|
Test Equipment |
Model Number |
|---|---|
|
Type-N (m) 50 ohm Termination |
909A Option 012 |
|
2.4 mm (f) 50 ohm Termination |
85138B |
|
|
In the following setups, cables are designated as solid lines and direct connections are designated as dashed lines. |