NFA — N8973B/74B/75B with frequency option ≤ 526
This adjustment determines the frequency at which the AC Coupling capacitor attenuates the input signal 3 dB. This frequency is stored in memory and the analyzer applies the appropriate correction for the capacitor rolloff.
Click here for troubleshooting.
|
Test Equipment |
Recommended Model Number |
|---|---|
|
Function Generator |
33622A |
|
BNC Cable |
8120-1840 |
|
Type-N (m) to BNC (f) adapter |
1250-1476 |
|
|
In the following setups, cables are designated as solid lines and direct connections are designated as dashed lines. |