IF Frequency Response UWBIF Full Bypass Path Adjustment

This adjustment applies to the following models:

The goal of this adjustment is to generate corrections for the IF band shape in Full Bypass Path (Option FBP). Option FBP allows both LNP and MPB to be enabled. A separate set of IF corrections are necessary for this RF Path. Since Full Bypass Path only affects frequencies above 3.6 GHz, only Bands 1, 2, 3, 4, 5, 6 are adjusted. This adjustment takes several hours, so it was separated from the same adjustment for Preselector Bypass Path (Option MPB).

In this adjustment, a –10.00 dBm signal is applied to the DUT. A reference amplitude is taken at the IF center frequency. The source frequency is then changed to a series of offset frequencies within the span of the IF. At each offset frequency, the input amplitude is maintained at –10.00 dBm, and the signal amplitude is measured by the DUT. The offset amplitude is subtracted from the reference amplitude. The resulting envelope created by all the offset amplitudes is the uncorrected IF Frequency Response.

Click here for troubleshooting.

Required Test Equipment

Test Equipment

Recommended Model Number

Network Analyzer1, 2

N5247B

  • Refer to the N7814A Readme for PNA firmware requirements.

Cable, BNC (m) to BNC (m)

8120-1840

Cable, 2.4 mm (f) to 2.4 mm (m)

8121-2065 (or equivalent)

Adapter, 2.4 mm (f) to 2.4 mm (f)

11900B (or equivalent)

  1. A calibration must be performed on the network analyzer prior to running the adjustment (see below).

  2. PNA preference setting recommendation: Unselect Power: Force RF Power Off at the end of the sweep

Network Analyzer Calibration Procedure

The network analyzer used in this adjustment must be calibrated prior to running the adjustment. The calibration will need to be repeated once every three days or if the connectors or cables have been disturbed. If it's been within the three day time frame and the connectors and cables have not been disturbed, then the network analyzer calibration is not necessary and you may proceed with the adjustment.

For a list of required equipment and calibration instructions to perform the network analyzer calibration, refer to Network Analyzer Freq Sweep Calibration.

Connection Setups

In the following setups, cables are designated as solid lines and direct connections are designated as dashed lines.