Freq Resp Low Noise Path Adjustment Overview

(UXA N9040B)

This adjustment has different test configurations depending on the frequency option of the DUT.

Choose the appropriate topic page link from the table below that matches the frequency option of the DUT.

Model Number

Frequency Options

 

N9040B

508 — 8.4 GHz
513 — 13.6 GHz
526 — 26.5 GHz

Click Here

N9040B

544 — 44 GHz
550 — 50 GHz

Click Here