All X-Series models
The instrument is turned ON, set to Internal Reference mode, and allowed to warm up for 30 minutes (except for CXA with Option PFR is 15 minutes and all other models with Option PFR is 4 hours). The frequency of the 10 MHz Reference is measured at the DUT's rear-panel port using a frequency counter which is locked to a primary frequency standard. The measured value is compared to the allowable offset guideline and is included in the Performance Test printout.
Click here for troubleshooting.
Test Equipment |
Recommended Model Number |
---|---|
Universal Counter |
53230A |
Frequency Standard1 |
5071A |
BNC Cable (2 required) |
8120-1840 |
|
|
In the following setups, cables are designated as solid lines and direct connections are designated as dashed lines. |