PXA — N9030B with Option 107
In this test an audio analyzer or an ultra low distortion function generator output is connected to the DUT and a distortion measurement is performed by the DUT.
Click here for troubleshooting.
|
Test Equipment |
Recommended Model Number |
Alternative Model Number |
|---|---|---|
|
Audio Analyzer |
U8903B |
Stanford Research Ultra Low Distortion Function Generator Model DS360 |
|
BNC Cable |
8120-1840 |
10503A |
|
|
In the following setups, cables are designated as solid lines and direct connections are designated as dashed lines. |