|
Noise Density is only tested on the following:
UXA N9041B models will also run a separate test on Input 2. |
The Noise Density test is performed at specified center frequencies. The noise marker is used to measure the dBm/Hz. The Input Noise Density is then calculated based on the instrument’s settings. The test is performed in I/Q Analyzer mode as this is the only mode available in Wideband IF.
Click here for troubleshooting.
|
Test Equipment |
Recommended Model Number |
|---|---|
|
50 ohm Termination |
909A, Option 012 |
|
2.4 mm (f) Termination |
85138B |
|
3.5 mm (f) Termination |
909D |