All X-Series models
|
UXA N9041B models will also run a separate test on Input 2. |
Residual Responses are discrete responses that appear on the analyzer display with no signal applied. They are created within the analyzer by the frequency synthesis and frequency conversion processes. Residuals are the result of imperfect shielding of internal signals, or by other unknown mechanisms.
In this test, the analyzer’s RF input is terminated with 50 ohms and the attenuator is set to 0 dB. The analyzer is tuned to known residual frequencies.
Click here for troubleshooting.
Test Equipment |
Recommended Model Number |
---|---|
50 ohm Type-N Termination |
909A Option 012 |
50 ohm Termination |
909D |
2.4 mm (f) Termination |
85138B |