Phase Noise Troubleshooting
Related Adjustments
If the Phase Noise test fails, check the results
of the DANL TEST. If DANL is out of spec, there is a good possibility
that the high average noise level is causing the noise sidebands test
to indicate a false failure.
Phase Noise is a parameter that describes short term instability of
LO tune frequency. Phase Noise appears as modulation sidebands near the
LO. The modulation source is noise within the LO Phase Lock Loop.
A Phase Noise failure would indicate that noise is being injected into
the LO Phase Lock Loop. The assembly most likely to be the source of the
failure would be the A14 L.O. Synthesizer Assembly.
Failures at the 100 Hz offset are usually caused by AC line related
(100 Hz/120 Hz) spurs. If a distribution amplifier is being used to distribute
the analyzer 10 MHz to multiple sources, remove it from the path. Distribution
amplifiers tend to add AC power related spurts to the reference signal.
Failures at the 10 MHz offset have been caused by leaving an external reference connected to the DUT's EXT REF IN port. The external reference can cause a spur to appear at the 10 MHz offset.
Another, but least likely, assembly that could
cause a Phase Noise failure would be the A13 Front End Assembly.
|