Frequency Reference Accuracy TroubleshootingRelated AdjustmentsIf the adjustment does not solve the problem, suspect a faulty A16 Reference assembly. If the result was Undetermined and the 10 MHz External Reference was used, verify that the accuracy of the 10 MHz Reference was updated in TME in the Additional Properties function. Refer to the Additional Properties section in the N7800A TME Help for instructions. |