Residual Responses Troubleshooting
Related Adjustments
If the residuals test fails, check the results of the DANL TEST. If
DANL is out of spec, there is a good possibility that the high average
noise level is causing the residuals test to indicate a false failure.
Also assure the 50 ohm load is attached to
the analyzer RF Input connector. Failures are usually caused by loose
or defective cables or loose shielding on an assembly. See the analyzer
Service Guide for troubleshooting information.
|