Internal Alignment TroubleshootingAn internal alignment failure suggests that there is an internal hardware failure that should be repaired. If an internal alignment failure has occurred, the specific errors can be viewed on the MXE by pressing System-Show Errors. Please refer to the Instrument Messages and Functional Tests Guide for error message descriptions. |