Second Harmonic Distortion Troubleshooting
Failures when the source frequency is less than or equal to 1.8 GHz
are usually a low band path problem. Suspect the A13 Front End Assembly
or something between the input connector and the Front End assembly.
Lowband measurements are performed with an external low-pass filter
in the signal path. The low pass filters are used to reduce the second
harmonic of the signal source. If the analyzer fails at < 1.8 GHz,
the filters may be suspect.
Failures when the source frequency is greater
than 3.6 GHz are usually a high band problem. Suspect the A12 YTF or something
between the input connector and the YTF assembly. See the MXE Service Guide for troubleshooting information.
|