Peak, Ave, RMS Troubleshooting

The detectors are implemented in DSP.

A test failure is most likely caused by the test system (as opposed to a hardware fail). The source requires Option UNW Narrow Pulse to generate the Pulsed RF signal. The PSG Option UNW is specified down to 50 MHz.

This test requires a Pulsed RF signal at 125 kHz which is an unspecified range of the pulse modulator.  The E8267D signal generator tends to have more issues than the E8257D. If a failure occurs, try using the E8257D signal generator.