Sine Wave Accuracy Troubleshooting

If a failure occurs on the Sine Wave accuracy test, then there are several possible reasons:

  1. The test setup has loose or damaged connectors. Check to make sure the cable and connectors are not damaged

  2. The power meter sensor calibration data is not correct. The power sensor requires calibration data which is in the test station information. If the sensor data is incorrect, the power meter will not read the proper power levels.

  3. The MXE flatness corrections are not correct. Please refer to the MXE Service Guide for more information.