This calibration adjusts the output power to be flat across frequencies greater than 3.2 GHz, but less than or equal to 50 GHz. Also, the accuracy of the output power is adjusted when the step attenuator is set at various levels. For digital units, the attenuator is set at -5, -10, -15, -20, and -25 dB. For analog units, the attenuator is set to -5, -15, and -25 dB.
Test Equipment |
Preferred Model |
Alternate Model(s) |
Power Meter |
N1914A1 |
E4419B |
Power Sensor |
N8487A (50 GHz)2 |
E9300A H25 (24 GHz)2 |
Function Generator |
33250A |
33120A Opt 001 |
|
|
Connect all test equipment as shown.
Connect GPIB cables to all GPIB-controlled test equipment.
While performing this adjustment, follow all instructions on the controller display.
Setup for Power Meter Calibration
Setup for High Band Power Flatness Calibration
Setup for High Band Power Flatness Calibration (E8267D Only)
If this adjustment fails, perform the following steps in order:
Check the equipment setup (see above). If the setup is incorrect, make the necessary corrections and rerun the adjustment.
If this adjustment fails with the equipment set up properly, refer to the troubleshooting section of the signal generator's service guide. If you do not have a printed copy of the service guide (Option OBW), one is available either on the CD-ROM that came with your signal generator shipment or on the Keysight Website.
If you cannot correct the problem using the troubleshooting procedures in the Service Guide, obtain service from Keysight Technologies. Refer to Contacting Keysight Technologies.