This power flatness calibration adjusts the output power to be flat in the analog low frequency output mode by taking the path correction measurements at +10 dBm and -10 dBm across the frequency range from 9 KHz to 1 MHz. The corrections are saved into "ANALOG LF AS RF GAIN HIGH" and "ANALOG LF AS RF GAIN LOW" arrays. During calibration, the LF Output is switched to the RF chain path.
|
Test Equipment |
Preferred Model |
Alternate Model(s) |
|
Power Meter |
N1914A1 |
E4419B |
|
Power Sensor |
E9304A H19 (18 GHz) |
|
|
|
|
Connect all test equipment as shown.
Connect GPIB cables to all GPIB-controlled test equipment.
While performing this adjustment, follow all instructions on the controller display.
Setup for Power Meter Calibration
Setup for Low Frequency Output Power Flatness Calibration
If this adjustment fails, perform the following steps in order:
Check the equipment setup (see above). If the setup is incorrect, make the necessary corrections and rerun the adjustment.
If this adjustment fails with the equipment set up properly, refer to the troubleshooting section of the signal generator's service guide. If you do not have a printed copy of the service guide (Option OBW), one is available either on the CD-ROM that came with your signal generator shipment or on the Keysight Website.
If you cannot correct the problem using the troubleshooting procedures in the Service Guide, obtain service from Keysight Technologies. Refer to Contacting Keysight Technologies.