This adjustment calibrates the GAIN ADJUST DAC on the A8 Output. This GAIN ADJUST DAC is used to control the RF power level that is incident upon the switched filters and subsequent RF amplifiers by setting the control point for the gain adjust modulator. This calibration ensures that there will be sufficient power available at the RF amplifiers to perform the desired modulation while minimizing intermodulation distortion when the digital modulation is achieved. After adjustment, the results are stored in the signal generator.
|
Test Equipment |
Preferred Model |
Alternate Model(s) |
|
Power Meter |
N1914B |
N1914A1 |
|
Power Sensor |
E9304A Opt H19 |
|
|
Function Generator |
33622A |
33611A |
|
|
|
Connect all test equipment as shown.
Connect GPIB cables to all GPIB-controlled test equipment.
While performing this adjustment, follow all instructions on the controller display.
Setup for Power Meter Calibration
Setup for Low Band Digital Gain Calibration
Setup for Low Band Digital Gain Calibration (E8267D with Option H16, 016, HBQ, or HBR)
If this adjustment fails, perform the following steps in order:
Check the equipment setup (see above). If the setup is incorrect, make the necessary corrections and rerun the adjustment.
If this adjustment fails with the equipment set up properly, refer to the troubleshooting section of the signal generator's service guide. If you do not have a printed copy of the service guide (Option OBW), one is available either on the CD-ROM that came with your signal generator shipment or on the Keysight Website.
If you cannot correct the problem using the troubleshooting procedures in the Service Guide, obtain service from Keysight Technologies. Refer to Contacting Keysight Technologies.