Use this calibration to optimally set the prelevel reference DAC on the output board for use in the digital mode of operation.
The prelevel reference DAC on the output board is used to control the RF power level that is incident upon the I/Q modulator. It does this by setting the control point for the prelevel loop. The loop has a detector on an output of the I/Q modulator. Its drive circuitry is also on the output board, but the RF modulator that it controls is on the Frac-N/synthesizer board. The goal of this calibration is to have sufficient power available at the I/Q modulator to perform the desired modulation—and have enough DUT output power available—while minimizing intermodulation distortion when digital modulation is in use.
|
Test Equipment |
Preferred Model |
Alternate Model(s) |
|
Power Meter |
N1914A1 |
E4419B |
|
Power Sensor |
E9304A Opt H19 |
E9304A |
|
|
|
Setup for Power Meter Calibration
Setup for Low Band Digital Prelevel Calibration
If this adjustment fails, perform the following steps in order:
Verify that the GPIB cable is connected between the controller and the signal generator being calibrated and rerun the adjustment.
If this adjustment still fails after step 1, refer to the troubleshooting section of the signal generator's service guide. If you do not have a printed copy of the service guide (Option OBW), one is available either on the CD-ROM that came with your signal generator shipment or on the Keysight Website.
If you cannot correct the problem using the troubleshooting procedures in the Service Guide, obtain service from Keysight Technologies. Refer to Contacting Keysight Technologies.