The Low Band Power Maximum Calibration adjusts the Amp Filter board step attenuator.
|
Test Equipment |
Preferred Model |
Alternate Model(s) |
|
Power Meter |
N1914A1 |
E4419B |
|
Power Sensor |
E9304A H192 |
N8481H CFT3 |
|
|
|
Connect all test equipment as shown.
Connect GPIB cables to all GPIB-controlled test equipment.
While performing this adjustment, follow all instructions on the controller display.
Setup for Power Meter Calibration
Setup for Low Band Power Maximum Calibration
If this adjustment fails, perform the following steps in order:
Check the equipment setup (see above). If the setup is incorrect, make the necessary corrections and rerun the adjustment.
If this adjustment fails with the equipment set up properly, refer to the troubleshooting section of the signal generator's service guide. If you do not have a printed copy of the service guide (Option OBW), one is available either on the CD-ROM that came with your signal generator shipment or on the Keysight Website.
If you cannot correct the problem using the troubleshooting procedures in the Service Guide, obtain service from Keysight Technologies. Refer to Contacting Keysight Technologies.