This adjustment calibrates the power at the output of the I/Q multiplexer board that results in optimum adjacent channel power ratio. The adjustment is dependent on prior ALC and I/Q calibrations.
Targeted I/Q power is determined by the intersection of the distortion and noise curves exhibited by the output of the I/Q modulator. With known slopes for Distortion vs. I/Q Multiplexer Output Power and Noise vs. I/Q Multiplexer Output Power, an intersection point of the curves is determined and the I/Q power is set so that it does not exceed the optimum power level.
|
Test Equipment |
Preferred Model |
|
|
Spectrum Analyzer |
E444xA1 |
|
|
External Baseband Signal Generator |
E4438C Opt 402 and (001, 002, 601, or 602) |
E8267D Opt (601 or 602) |
1.Select any model of PSA spectrum analyzer (E4440A, E4443A,E4445A, E4446A, E4447A, E4448A) that has a maximum frequency greater than or equal to the maximum frequency of the unit under test. An E4448A is required for units with Option 567. The E4448A frequency range is adequate for all PSG-D frequency configurations.
|
|
|
Connect all test equipment as shown.
Connect GPIB cables to all GPIB-controlled test equipment.
While performing this adjustment, follow all instructions on the controller display.
Setup for Target I/Q Power Calibration (Option 601, 602 Only)
Setup for Target I/Q Power Calibration (All models without Option 601,602)
If this adjustment fails, perform the following steps in order:
Check the equipment setup (see above). If the setup is incorrect, make the necessary corrections and rerun the adjustment.
Please check and ensure that the 856XE/EC series spectrum analyzer's external reference is connected. The spectrum analyzer will lock up and not take a sweep when external reference is selected and there isn't one connected to it.
If this adjustment fails after step 1 and step 2, refer to the troubleshooting section of the signal generator's service guide. If you do not have a printed copy of the service guide (Option OBW), one is available either on the CD-ROM that came with your signal generator shipment or on the Keysight Website.
If you cannot correct the problem using the troubleshooting procedures in the Service Guide, obtain service from Keysight Technologies. Refer to Contacting Keysight Technologies.