This calibration adjusts the output power to be flat across frequencies greater than 50 GHz. Also, the accuracy of the output power is adjusted when the step attenuator is set at -5, -15, and -25 dB.
Test Equipment |
Preferred Model |
Alternate Model(s) |
Power Meter |
N1914A1 |
E4419B |
Power Sensor |
V8486A H67 (67 GHz)2 |
|
|
|
Connect all test equipment as shown.
Connect GPIB cables to all GPIB-controlled test equipment.
While performing this adjustment, follow all instructions on the controller display.
Setup for Power Meter Calibration
Setup for V-Band Power Flatness Calibration
If this adjustment fails, perform the following steps in order:
Check the equipment setup (see above). If the setup is incorrect, make the necessary corrections and rerun the adjustment.
If this adjustment fails with the equipment set up properly, refer to the troubleshooting section of the signal generator's service guide. If you do not have a printed copy of the service guide (Option OBW), one is available either on the CD-ROM that came with your signal generator shipment or on the Keysight Website.
If you cannot correct the problem using the troubleshooting procedures in the Service Guide, obtain service from Keysight Technologies. Refer to Contacting Keysight Technologies.