This adjustment is an operation that backs up the entire file system and all calibration data to the motherboard memory. It is optional and does not have to be run. The user may choose to run this adjustment to backup calibration data after other adjustments have succeeded.
When to backup:
When not to backup:
If adjustments have not completed or if performance tests do not pass.
|
|
Performing a backup under these conditions will overwrite factory defaults which cannot be recovered by the user. |
When to restore from backup:
Refer to the Service Guide for related information.
Connect a GPIB cable between the controller and the signal generator being calibrated.
While performing this adjustment, follow all instructions on the controller display.
If this adjustment fails, perform the following steps in order:
Verify that the GPIB cable is connected between the controller and the signal generator being calibrated and rerun the adjustment.
If this adjustment still fails after step 1, refer to the troubleshooting section of the signal generator's service guide. If you do not have a printed copy of the service guide (Option OBW), one is available either on the CD-ROM that came with your signal generator shipment or on the Keysight Website.
If you cannot correct the problem using the troubleshooting procedures in the Service Guide, obtain service from Keysight Technologies. Refer to Contacting Keysight Technologie.