High Band IQ Power Floor Calibration

(E8267D Only)

This adjustment determines the power level out of the I/Q MUX assembly; this power level sets the RF output power to the top of the digital vernier range.

Required Test Equipment

Test Equipment

Preferred Model

Alternate Model(s)

Power Meter

N1914B

N1914A1
E4419B
E4419A

Power Sensor

E9300A Opt H25

N8487A
8487A Opt H842
N8485A
N8485A CFT
8485A Opt H842

Function Generator

33622A

33611A
33612A
33621A
33250A
33120A Opt 001

  1. Power meter N1914A with serial numbers ranging between MY00000000—MY53040007 require Service Note 07 to be applied for measurement repeatability. Please have this service note applied or verify it was applied before using this power meter. The affected service note is: N1914A-07 Service Note
  2. Option H84 provides reflection coefficient data.

 

Connections and Setup Procedures

  • All test equipment requires a 30 minute warmup period to ensure accurate performance.

  • In the following test setup, cables are designated as solid lines and direct connections are designated as dashed lines.

  1. Connect all test equipment as shown.

  2. Connect GPIB cables to all GPIB-controlled test equipment.

  3. While performing this adjustment, follow all instructions on the controller display.

 

Setup for Power Meter Calibration

 

 

Setup for I/Q Power Floor Calibration

 

 

In Case of Difficulty

If this adjustment fails, perform the following steps in order:

  1. Check the equipment setup (see above). If the setup is incorrect, make the necessary corrections and rerun the adjustment.

  2. If an "IQ Calibration Failed" error dialog occurs at the beginning of the adjustment, manually run the IQ calibration using the front panel and observe the errors on the DUT. If successful, repeat the test.

  3. If this adjustment fails with the equipment set up properly, refer to the troubleshooting section of the signal generator's service guide. If you do not have a printed copy of the service guide (Option OBW), one is available either on the CD-ROM that came with your signal generator shipment or on the Keysight Website.

  4. If you cannot correct the problem using the troubleshooting procedures in the Service Guide, obtain service from Keysight Technologies. Refer to Contacting Keysight Technologies.