A DC voltage is used to switch the DUT pulse modulation on and off. A spectrum analyzer is used to measure the power of the fundamental (CW) frequency of the DUT with the pulse On and Off. The difference in these power levels is the Pulse On/Off ratio, in dB
|
Test Equipment |
Recommended Models |
Alternative Models |
|
Spectrum Analyzer |
N9030B Opt 5xx1 |
N9030A Opt 5xx1 E444xA2 |
|
Function Generator |
33622A |
33611A |
|
|
|
|
Connect all test equipment as shown.
Connect GPIB cables to all GPIB-controlled test equipment.
While performing this performance test, follow all instructions on the controller display.
Setup for Pulse Modulation On/Off Ratio
If this performance test fails, perform the following steps in order:
Check the equipment setup (see above). If the setup is incorrect, make the necessary corrections and rerun the Performance Test.
If a 856xE/EC series spectrum analyzer is being used and the test locks up, please check and ensure that the 856xE/EC's external reference is connected. The spectrum analyzer will lock up and not take a sweep when external reference is selected and there isn't one connected to it.
If this test fails with the equipment setup properly, refer to the troubleshooting section of the signal generator's service guide. If you do not have a printed copy of the service guide (Option OBW), one is available either on the CD-ROM that came with your signal generator shipment, or on the Keysight Website.
If you cannot correct the problem using the troubleshooting procedures in the Service Guide, obtain service from Keysight Technologies. Refer to Contacting Keysight Technologies.