Error Vector Magnitude (EVM) is the magnitude of the vectorial difference between the measured signal and an ideal reference signal in the I-Q plane.
This test supports two different test setups using either a PXA signal analyzer or an 89441A VSA spectrum analyzer.
A PXA signal analyzer is used with the 89600 Vector Signal Analysis Application to measure EVM.
|
Test Equipment |
Critical Specifications for this Test |
Recommended Models |
Alternate Model(s) |
|
Signal Analyzer |
EVM Accuracy |
N9030B Opt 5xx1, MPB2 |
N9030A Opt 5xx1, MPB2 |
|
Vector Signal Analysis Application |
|
89600 VSA with these options3:
|
|
Alternatively, an 89441A vector spectrum analyzer (VSA) is used to measure EVM and Global Phase Error. When using the VSA, additional equipment is required for downconverting the signal above 2.65 GHz.
|
Test Equipment |
Critical Specifications for this Test |
Recommended Models |
Alternate Model(s) |
|
Vector Signal Analyzer |
None |
89441A Opt AYA, AYH, AY9, and UFG or UTH |
|
|
Local Oscillator1 |
Max Frequency of Local Oscillator must be greater than or equal to the Unit Under Test. |
E8257D2 Opt (1EA or 1EU) and (UNR, UNX, or UNY) |
E8267D (UNR, UNX, or UNY) E824xA/5xA Opt 1EA and UNJ E82x7C Opt 1EA and UNR E8267C Opt UNR |
|
Mixer |
None |
Marki M4-0265 |
0955-2225 (Only for Opt 520) |
|
10 dB Attenuator |
None |
8490D Opt 010 |
8493C Opt 010 (Only for E8267D Opt 520) |
|
|
|
|
|
|
Install the 89600 Vector Signal Analysis Application on the same PC as TME. This PC must also be connected to the LAN.
Connect the PXA signal analyzer to the LAN.
Get the Hostname or IP address of the PXA via the PXA’s front panel information system: System > Show > System.
Add the PXA to the LAN interface.
Open the Agilent Connection Expert for the Agilent IO libraries. If a LAN interface does not exist, add it:
Add the PXA as an instrument on this interface using the IP address from step 3.
Verify that the instrument has been successfully added to the interface.
|
|
See below for troubleshooting tips if using VSA software 89601B version 21.0 or greater with Keysight IO libraries. |
Open the Keysight Connection Expert for the Keysight IO libraries and add the PXA to a LAN interface by selecting Manual Configuration > Add New Instrument/Interfaces > LAN instrument.
Add the PXA as a LAN device by entering the PXA's Hostname (preferred method) or IP address as shown below.
|
|
Using the PXA's Hostname is the preferred method to avoid the possibility of crashing the software. The Hostname can be found in the PXA's System menu. An example of a Hostname is: K-N9030B-80323, where K = Keysight, N9030B = model, 80323 = last 5 digits of the serial number. |
Verify the instrument address by selecting Test This VISA Address, then select Accept.
Ensure the equipment is connected as shown:
If this performance test fails, perform the following steps in order:
Check the equipment setup (see above). If the setup is incorrect, make the necessary corrections and rerun the Performance Test.
If this test fails with the equipment setup properly, check and ensure that the local oscillator (LO) meets its phase noise specifications by performing a phase noise measurement at the LO frequency the EVM is failing at.
If an "IQ Calibration Failed" error dialog occurs at the beginning of the test, manually run the IQ calibration using the front panel and observe the errors on the DUT. If successful, repeat the test.
If this test still fails after steps 1, 2, and 3, refer to the troubleshooting section of the signal generator's service guide. If you do not have a printed copy of the service guide (Option OBW), one is available either on the CD-ROM that came with your signal generator shipment or on the Keysight Website.
If you cannot correct the problem using the troubleshooting procedures in the Service Guide, obtain service from Keysight Technologies. Refer to Contacting Keysight Technologies.
When adding the PXA as LAN device, use the PXA's Hostname rather than the IP Address to avoid the possibility of crashing the software. The Hostname can be found in the PXA's System menu. An example of a Hostname is: K-N9030B-80323, where K = Keysight, N9030B = model, 80323 = last 5 digits of the serial number.
If the VSA software freezes during the Digital Modulation Quality test, manually verify that the you are able to “Rediscover Instruments” in the VSA software.
Next, click on the Discover Instruments tab and click on the Rediscover Instruments button.
If this freezes, then you may need to set the Keysight VISA as the Preferred VISA. To set the Keysight VISA as the preferred VISA:
Open the Keysight Connection Expert and go to Settings > Visa Conflict Manager > General VISA Settings. Ensure Keysight VISA is set as the preferred VISA implementation as shown in the image below: