This manual test verifies that the signal generator's residual phase noise meets specifications.
Residual phase noise is the phase noise of the signal generator excluding the contribution of the 10 MHz reference.
With the N5511A Phase Noise Test System (PNTS), the 10 MHz out of the of the M9300A frequency reference is split to provide a common reference signal to both the reference signal generator and to the test signal generator.
When using a legacy phase noise test system (E5505A, E5504A/B, or E5503A/B), the N5507A or 70427A downconverter's buffered 10 MHz output signal is used.
For test signal generators with Option UNX, an E82x7D with Option UNX or UNY is used as the reference source. For test signal generators with Option UNY, only an E82x7D with Option UNY can be used as the reference source.
|
Test Equipment |
Recommended Models |
Alternate Model(s) |
|
Phase Noise System |
N5511A Options 540, CH21
|
E5505A Option 001
|
|
Reference Source |
E8257D Opt UNT, UNY, 1EU E8257D/E8663D Opt HY21
|
E8257D Opt UNT, UNR1 or UNX1 or HNY3, and 1EU E8663D Opt UNT, UNX1 or UNY and 1EU
|
|
Power Splitter |
Mini-Circuits ZFSC-2-2-S+ (Keysight part number 0955-2274) |
|
|
3 dB Attenuator |
8490D Opt 003 |
8491x Opt 003 |
|
6 dB Attenuator
|
8490D Opt 006 |
8491x Opt 006 |
There are two sets of procedures depending on the model of the phase noise test system used:
E5505A, E5504A/B, and E5503A/B, legacy phase noise test systems
Select from the links below according to the phase noise test system being used.
Connect all test equipment as shown.
For the 10 MHz connections:
Connect the outputs of the power splitter to the 10 MHz frequency reference of both the DUT and the Reference Source.
Connect GPIB cables to all GPIB-controlled test equipment.
Preset all test equipment and the DUT.
Change the following parameters in the N5510A PNTS user interface:
Select the View pull-down menu.
Select Display Preferences and un-check the Spurs box.
Select OK to close Display Preferences.
Select the System pull-down menu and select Server Hardware Connections.
Select or ensure the following:
FFT Analyzer has Keysight M9551A selected.
Select Close to close Server Hardware Connections.
Select the Define
pull-down menu, select Measurement, and select the
following settings:
|
Parameter |
Setting |
|
|
|
|
Type and Range Tab |
|
|
Measurement Type |
Absolute phase noise (using a phase locked loop) |
|
Measurement Method |
Fast |
|
Start Offset Resolution Expansion |
10 |
|
Channel Setup |
Single |
|
Start Offset Frequency |
9 Hz (must be < first specified offset frequency) |
|
Stop Offset Frequency |
110 kHz (must be > last specified offset frequency) |
|
FFT Analyzer Minimum Number of Trace Averages |
160 |
|
RBW % |
1.96 (1024 point FFT) |
|
FFT Overlap % |
75 |
|
FFT Window Type |
Flat Top |
|
|
|
|
Sources Tab |
|
|
Carrier Source Frequency |
Obtain tested frequencies from the TME data entry form. |
|
Carrier Source Power |
+10 dBm |
|
Detector Input Frequency |
Same as Carrier Source Frequency |
|
Reference Source Power |
+15 dBm |
|
VCO Nominal Tune Constant |
1 Hz/Volt |
|
VCO Tune Range |
1 Volt |
|
VCO Input Resistance |
50 Ω |
|
Center Voltage |
0 |
|
|
|
|
Cal Tab |
|
|
Phase Detector Constant |
Derive detector constant from measured beat note |
|
VCO Tune Constant |
Measure VCO Tune Constant |
|
Verify calculated phase lock loop suppression |
Blank |
|
|
|
|
Block Diagram Tab |
|
|
Carrier Source |
Manual |
|
Reference Source |
Model number of reference source |
|
Phase Detector |
Automatic Detector Selection |
|
Test Set Tune Voltage Output |
Front Panel |
|
Test Set Tune Voltage Destination |
Reference Source |
|
VCO Tune Mode |
DCFM |
|
|
|
|
Test Set Tab |
|
|
LNA Low Pass Filter |
Internal — Selected Auto — Checked |
|
LNA Gain |
Auto Gain — Selected Minimum Auto Gain — 14 dB |
|
PLL Integrator Attenuation |
0 dB |
|
Use Channel #2 |
Unchecked |
|
|
|
|
Graph Tab |
|
|
Title |
User specified |
|
Graph Type |
Single-sideband phase noise (dBc/Hz) |
|
X Scale minimum |
Same as start offset frequency |
|
X Scale maximum |
Same as stop offset frequency |
|
Y Scale maximum |
0 dBc/Hz |
|
Y Scale minimum |
–170 dBc/Hz |
|
Normalize Trace Data |
1 Hz bandwidth |
|
Trace Smoothing Amount |
0 |
Making the Measurement
Set the DUT frequency to the first carrier frequency and power in the TME data entry form.
Set the DUT RF Output to On.
If testing a DUT with Option UNX, UNY, or HNY, ensure that the Optimize φ Noise is set to Optimize φ Noise Offset < 150 kHz (Mode 1). To do this, press Frequency > More > More > Optimize φ Noise and select Optimize φ Noise Offset < 150 kHz (Mode 1).
Select the Measure pull-down menu and select New Measurement.
When the measurement completes, select the Markers icon and place markers at specified offsets to determine the measured phase noise. When specifying a marker offset, the marker will be set to the closest frequency on the graph as indicated in the following table:
|
Nominal Offset |
Actual Offset |
|
10 Hz |
10.058 Hz |
|
100 Hz |
99.838 Hz |
|
1 kHz |
1.0014 kHz |
|
10 kHz |
9.9182 kHz |
|
20 kHz |
19.836 kHz |
|
100 kHz |
100.71 kHz |
|
|
All test equipment requires a 30 minute warmup period to ensure accurate performance. |
Connect all test equipment as shown.
Connect GPIB cables to all GPIB-controlled test equipment.
Preset all test equipment and the signal generator.
Connect the Reference Source E82x7D Option UNX/UNY/HNY RF Output to the N5500A or 70420A Reference Input.
Connect the N5507A or 70427A Down Converter's buffered 10 MHz output to the 3 dB attenuator and connect the attenuator to the input of the Mini-Circuits ZFSC-2 Power Splitter.
Connect one output port of the splitter to the rear panel 10 MHz Ref In of the reference source.
Connect the other output port of the splitter to the signal generator's rear panel 10 MHz Ref In.
Connect the N5500A or 70420A Tune Voltage Output to the front panel Ext 1 Input of the Reference Source E82x7D.
In the E5505A Phase Noise System user interface, change the following parameters:
Select the View pull down menu.
Select Display Preferencesand un-check the Spurs box.
Select OK to close Display Preferences.
Select the Define pull down menu, select Measurement, and select the following settings:
|
Parameter |
Setting |
||||||||||||||||||||||||||||||||||||||||||||||||||
|
|
|
||||||||||||||||||||||||||||||||||||||||||||||||||
|
Type and Range Tab |
|
||||||||||||||||||||||||||||||||||||||||||||||||||
|
Measurement Type |
Absolute phase noise (using a phse lock loop) |
||||||||||||||||||||||||||||||||||||||||||||||||||
|
Start Offset Frequency |
1 Hz |
||||||||||||||||||||||||||||||||||||||||||||||||||
|
Stop Offset Frequency |
100 MHz |
||||||||||||||||||||||||||||||||||||||||||||||||||
|
FFT Averages |
4 |
||||||||||||||||||||||||||||||||||||||||||||||||||
|
FFT Quality |
Custom |
||||||||||||||||||||||||||||||||||||||||||||||||||
|
Define Custom Segment Table - FFT Note: the following parameters should be left at their default values for all segments:
|
|
||||||||||||||||||||||||||||||||||||||||||||||||||
|
Swept Quality |
Normal |
||||||||||||||||||||||||||||||||||||||||||||||||||
|
|
|
||||||||||||||||||||||||||||||||||||||||||||||||||
|
Sources Tab |
|
||||||||||||||||||||||||||||||||||||||||||||||||||
|
Carrier Source Connected |
Test Set |
||||||||||||||||||||||||||||||||||||||||||||||||||
|
Carrier Source Frequency |
100, 500 MHz and 1, 2, 3.2 GHz |
||||||||||||||||||||||||||||||||||||||||||||||||||
|
Carrier Source Power |
For frequencies ≤ 2 GHz: +10 dBm or maximum specified power, whichever is less. Note: If the test frequency is > 1.2 GHz and <= 3.2 GHz, then add a 6 dB attenuator to the DUT RF output (not required for Option 550 or 567 models). For frequencies > 2 GHz: +5 dBm or maximum specified power, whichever is less. |
||||||||||||||||||||||||||||||||||||||||||||||||||
|
Detector Input Frequency |
Same as carrier source frequency |
||||||||||||||||||||||||||||||||||||||||||||||||||
|
Reference Source Power |
+15 dBm, or +10 dBm for frequencies > 1.2 GHz. |
||||||||||||||||||||||||||||||||||||||||||||||||||
|
VCO Tune Constant |
1 Hz/Volt |
||||||||||||||||||||||||||||||||||||||||||||||||||
|
VCO Tune Range |
1 Volt |
||||||||||||||||||||||||||||||||||||||||||||||||||
|
VCO Input Resistance |
50 ohms |
||||||||||||||||||||||||||||||||||||||||||||||||||
|
|
|
||||||||||||||||||||||||||||||||||||||||||||||||||
|
Cal Tab |
|
||||||||||||||||||||||||||||||||||||||||||||||||||
|
Measure Phase Detector Constant |
Checkmark |
||||||||||||||||||||||||||||||||||||||||||||||||||
|
Calculate from expected VCO Tune constant using tune port resistence |
Checkmark |
||||||||||||||||||||||||||||||||||||||||||||||||||
|
Verify calculated phase lock loop suppression |
Blank |
||||||||||||||||||||||||||||||||||||||||||||||||||
|
Phase Lock Loop Suppression |
Use Adjusted Values |
||||||||||||||||||||||||||||||||||||||||||||||||||
|
|
|
||||||||||||||||||||||||||||||||||||||||||||||||||
|
Block Diagram Tab |
|
||||||||||||||||||||||||||||||||||||||||||||||||||
|
Carrier Source |
Manual |
||||||||||||||||||||||||||||||||||||||||||||||||||
|
Down Converter |
None |
||||||||||||||||||||||||||||||||||||||||||||||||||
|
Reference Source |
E8257D Asset Control Module (use the E8257C if the E8257D is not available) |
||||||||||||||||||||||||||||||||||||||||||||||||||
|
Phase Detector Mode |
Automatic |
||||||||||||||||||||||||||||||||||||||||||||||||||
|
Test Set Tune Voltage Destination |
Reference Source |
||||||||||||||||||||||||||||||||||||||||||||||||||
|
VCO Tune Mode |
DCFM |
||||||||||||||||||||||||||||||||||||||||||||||||||
|
|
|
||||||||||||||||||||||||||||||||||||||||||||||||||
|
Test Set Tab |
|
||||||||||||||||||||||||||||||||||||||||||||||||||
|
Input Attenuation |
0 dB |
||||||||||||||||||||||||||||||||||||||||||||||||||
|
LNA Low Pass Filter |
Auto |
||||||||||||||||||||||||||||||||||||||||||||||||||
|
LNA Gain |
Auto |
||||||||||||||||||||||||||||||||||||||||||||||||||
|
PLL Integrator Attenuation |
0 dB |
||||||||||||||||||||||||||||||||||||||||||||||||||
|
|
|
||||||||||||||||||||||||||||||||||||||||||||||||||
|
Downconverter Tab |
|
||||||||||||||||||||||||||||||||||||||||||||||||||
|
Input Attenuation |
Auto |
||||||||||||||||||||||||||||||||||||||||||||||||||
|
IF Gain |
Auto |
||||||||||||||||||||||||||||||||||||||||||||||||||
|
Microwave/Millimeter Band |
Microwave (0 – 26.5 GHz) |
||||||||||||||||||||||||||||||||||||||||||||||||||
|
Reference Chain Reference |
10 MHz |
||||||||||||||||||||||||||||||||||||||||||||||||||
|
External Tune Enable |
Blank |
||||||||||||||||||||||||||||||||||||||||||||||||||
|
|
|
||||||||||||||||||||||||||||||||||||||||||||||||||
|
Graph Tab |
|
||||||||||||||||||||||||||||||||||||||||||||||||||
|
Title |
User specific |
||||||||||||||||||||||||||||||||||||||||||||||||||
|
Graph Type |
Single-sideband phase noise (dBc/Hz) |
||||||||||||||||||||||||||||||||||||||||||||||||||
|
X Scale minimum |
1 Hz |
||||||||||||||||||||||||||||||||||||||||||||||||||
|
X Scale maximum |
100E+6 |
||||||||||||||||||||||||||||||||||||||||||||||||||
|
Y Scale maximum |
0 |
||||||||||||||||||||||||||||||||||||||||||||||||||
|
Y Scale minimum |
-170 |
||||||||||||||||||||||||||||||||||||||||||||||||||
|
Normalize Trace Data |
1 Hz bandwidth |
Making the Measurement
Set the DUT frequency to 100 MHz and the power to +10 dBm or maximum specified power, whichever is less.
Select Utility > Instrument Adjustments > Reference Oscillator Adjustment > Restore Factory Defaults (Internal Ref. Bandwidth = 125 Hz, External Ref. Bandwidth = 650 Hz).
Set the DUT RF Output to On.
For a test signal generator with Option UNY, set Optimize φ Noise to Optimize φ Noise Offset < 150 kHz (Mode 1). To do this, select Frequency > More > More Optimize φ Noise.
For testing with an E8663D Option HY2, set Optimize Signal Noise Mode OFF. To do this, perform the following steps in order:
Press Frequency > More > Low Pass Filter Below 2 GHz and select Off.
Select the Measure pull down menu and select New Measurement.
If using a release of the phase noise measurement software older than A.04.05.0001, ensure the Input Impedance on the Reference Source’s Ext 1 Input is set to 50 Ohms. To do this, select FM/ φM > More > Ext Impedance and select 50 Ohm.
If using an HY2 equipped PSG-D as the reference source, ensure that SNR mode is disabled. To do this, perform the following steps:
Press Frequency > More > Low Pass Filter Below 2 GHz and select Off.
If the PLL Suppression Calibration Factors panel appears, select Continue using Adjusted Loop Suppression.
When the measurement completes, select the Markers icon and place markers at the offsets specified by TME. To get these offsets:
Launch TME with the DUT connected to the test system.
Start the Residual Phase Noise test.
With the form selected, press Ctrl-A, Ctrl-C on the keyboard to collect the data in the form.
Open an application such as Microsoft Notepad and press Ctrl-V to copy the test point data into this application.
Print out this data and use it to complete this test.
Compare the marker amplitude value to the specifications from the datasheet shipped with this product (also found with the data collected in step 6).
If a test point fails the measurement, then route the 10 MHz Oven Out from the N5507A downconverter to the input of the splitter and repeat the measurement.
| Note: If a failure occurs, a three-source comparison measurement should be performed at this carrier frequency and offset to identify a true failure. |
Print out a phase noise plot.
Continue to the next carrier frequency and perform the measurement. Note the following frequency specific changes:
At 2 GHz:
Move the reference source RF Output to the 1.2-26.5 GHz REF INPUT from the 50 kHz-1600 MHz REF INPUT.
Add a 6 dB attenuator to the DUT RF Output. (Not required for DUT Option 550 or 567.)
Change the reference source power to +10 dBm.
At 3 GHz:
Set the DUT power to +5 dBm or maximum specified power, whichever is less.
The measurement data must be entered into the following form displayed on-screen when the test is run.
Enter the measured value from the phase noise system into the "Measured Value" column for the appropriate frequency/offset frequency combination. All values must be entered for the test to complete. Entering a measured value and then clicking in the "Result" column in the form will cause the result to appear.
If the "Guardbanding On" checkbox is not selected, then the overall result would not include uncertainty to calculate PASS/FAIL result. Otherwise, the result will be calculated using the displayed uncertainty and will be in the form of PASS/FAIL/INDETERMINATE. The specification against which the measured value is compared is displayed in the "Specifications" column.