Smart Connection

Some performance tests have a smart connection feature that verifies the connections made to the test equipment and determines if the test can run with the current connections.

If the performance tests are run in the default sequence, or if the previous performance test uses the same connections, the connection prompt does not appear on the display.

When the performance test sequence starts, tests will perform a connection check. If the connection check passes, the connection prompt is not displayed and the performance test will proceed. This reduces the need for you to interact with the connection prompts when sequential tests have the same connection setup. If the connection check fails, the connection instructions will be displayed prompting you to make the connection.