This adjustment calibrates the AM path to remove any offsets generated when LIN AM, LIN BURST or LOG BURST are enabled. The calibration determines the ALC reference DAC ”delta” value which will correct the offset when the modulation is enabled. This value is stored in the appropriate cal constant. To calibrate each path, the UUT is set up with modulation off, the ALC reference DAC is set for mid-scale and a target power level measurement is made. Then the modulation is enabled and the ALC reference DAC is adjusted until the target value is met. The difference between the final DAC value and the mid-scale value is the calibration value. By setting the ALC reference DAC to mid-scale and using that as the beginning value, this calibration can be completed without a calibrated ALC loop.
|
Test Equipment |
Recommended Model |
Alternate Model |
|
Power Meter |
N1914B |
N1914A1 E4418A |
|
Power Sensor |
N8482A |
E9304A E9304A H18 N8482A CFT 8482A2 |
|
|
|
|
Power Meter and Power Sensor Calibration
If this adjustment fails, perform the following steps in order:
Check the equipment setup (see above). If the setup is incorrect, make the necessary corrections and rerun the adjustment.
If this adjustment fails with the equipment set up properly, refer to the troubleshooting section of the signal generator's service guide. If you do not have a printed copy of the service guide (Option OBW), one is available either on the CD-ROM that came with your signal generator shipment or on the Keysight Website.
If you cannot correct the problem using the troubleshooting procedures in the Service Guide, obtain service from Keysight Technologies. Refer to Contacting Keysight Technologies.