This calibration is used to adjust the bias modulator circuitry to provide an accurate logarithmic drop in power level for a linear input voltage. When correctly adjusted, a one volt signal on the input will result in a 40 dB drop in power level. The adjustment involves choosing the correct values for three DACs located in the burst modulator circuit. The adjustment is repeated at several frequencies and the results are stored in calibration arrays corresponding to each DAC.
The BURST MOD OFFSET DAC sets the initial current level through the burst modulator diode.
The BURST MODLIN DAC is used to calibrate the input voltage level to the burst driver circuit.
The BURST DRIVER BIAS/GAIN DAC sets the breakpoint at which the modulator switches from a logarithmic to a linear transfer function (”knee”).
|
Test Equipment |
Recommended Model |
Alternate Model |
|
Spectrum Analyzer |
N9030B Opt 5xx1 |
N9030A Opt 5xx1 E444xA2 Opt 233 |
|
Function Generator |
33622A |
33611A 33250A |
|
Digital Multimeter |
3458A Opt 002 |
34470A |
|
|
|
|
If this adjustment fails, perform the following steps in order:
Check the equipment setup (see above). If the setup is incorrect, make the necessary corrections and rerun the adjustment.
If this adjustment fails with the equipment set up properly, refer to the troubleshooting section of the signal generator's service guide. If you do not have a printed copy of the service guide (Option OBW), one is available either on the CD-ROM that came with your signal generator shipment or on the Keysight Website.
If you cannot correct the problem using the troubleshooting procedures in the Service Guide, obtain service from Keysight Technologies. Refer to Contacting Keysight Technologies.