When FM is enabled, voltage offsets on the reference and synthesizer boards appear as frequency shifts on the synthesizer VCO. This adjustment generates a DAC value to null the offsets associated with the various FM1 and FM2 paths on the reference board. There are two FM Offset DACs which generate a correction value for the external inputs, internal FM, and FM internally grounded. The two external inputs can either be AC or DC coupled. With all these different combinations, a total of 13 correction values are generated and stored in FlashROM.
This adjustment algorithm uses a frequency counter to measure the frequency
shifts of the VCO. The frequency counter is used to calculate the FM Offset
DAC sensitivity (DAC counts/Hz). The correction DAC value is then calculated
and stored in FlashROM.
|
Test Equipment |
Recommended Model |
Alternate Model |
|
Frequency Counter |
53230A Opt [106 or 115] |
53132A Opt 010 and [050 or 124] |
|
|
|
If this adjustment fails, perform the following steps in order:
Check the equipment setup (see above). If the setup is incorrect, make the necessary corrections and rerun the adjustment.
If this adjustment fails with the equipment set up properly, refer to the troubleshooting section of the signal generator's service guide. If you do not have a printed copy of the service guide (Option OBW), one is available either on the CD-ROM that came with your signal generator shipment or on the Keysight Website.
If you cannot correct the problem using the troubleshooting procedures in the Service Guide, obtain service from Keysight Technologies. Refer to Contacting Keysight Technologies.