This adjustment uses an internal firmware routine to perform this calibration. After the internal routine is complete the temporary calibration files from that routine are copied over to permanent storage. The internal firmware routine performs the tasks in the description below.
The purpose of this calibration is to determine the required I/Q gain, offset and quadrature calibration constant and array values that will minimize the I/Q modulation imperfections on the signals that the instrument provides. This program uses internal voltage sources and internal voltage detectors (on the I/Q Mux board and on the internal baseband generator board), measured by the internal ABUS, to perform the calibration. No external equipment is required (other than the controlling computer).
The calibrations performed by this program can be broken down into the following major sections:
Major Calibration Algorithm Sections
First, the program determines the I/Q Mux Board RMS-DC Converter Offset Imbalance compensation calibration constants.
Second, the program determines the I/Q Mux Board Main Path and External Output Path Attenuator non-linearity compensation calibration constants.
Third, the program determines the frequency-dependent I/Q Offset Imbalance compensation and Quadrature Imbalance compensation calibration constants associated with the I/Q modulator(s) and switchable filter paths on the Output Board(s).
Fourth, the program determines all of the I/Q Offset Imbalance compensation calibration constants associated with each of various paths through the I/Q Mux board. If the instrument has a baseband generator (BBG) installed, the I/Q Offset terms associated with it are also determined.
Fifth, the program determines the I/Q Gain Imbalance compensation calibration constants for the I/Q Mux Board. If the instrument has a BBG installed, the I/Q Gain Balance terms associated with it are also determined.
Sixth, the program determines the frequency-dependent I/Q Gain Imbalance compensation calibration constants associated with the I/Q modulator(s) and switchable filter paths on the Output Board(s).
|
Test Equipment |
Recommended Model |
|
50 ohm Termination |
909A Opt 012 |
|
|
|
If this adjustment fails, perform the following steps in order:
Check the equipment setup (see above). If the setup is incorrect, make the necessary corrections and rerun the adjustment.
If this adjustment fails with the equipment set up properly, refer to the troubleshooting section of the signal generator's service guide. If you do not have a printed copy of the service guide (Option OBW), one is available either on the CD-ROM that came with your signal generator shipment or on the Keysight Website.
If you cannot correct the problem using the troubleshooting procedures in the Service Guide, obtain service from Keysight Technologies. Refer to Contacting Keysight Technologies.