|
|
This adjustment requires firmware revision C.03.10 or later. |
The purpose of this calibration is to determine the I/Q timing skew adjustments required to minimize the I/Q timing skew of internally generated signals on the I/Q external outputs. This adjustment will be required for a number of the unique I/Q baseband paths that exist from the baseband generator through the instrument to the I/Q outputs.
The calibration is accomplished by applying identical multitone baseband signals to the I channel, the Q channel, but 180 degrees out of phase. The I/ Q outputs are then summed together through a tee and the resultant waveform is measured with a spectrum analyzer. The I/Q time skew between the I and Q channels is then adjusted until the signals cancel each other to the maximum extent possible. This point of maximum cancellation will coincide with the point at which the I and Q channels I/Q time skew is minimized.
|
Test Equipment |
Recommended Models |
Alternate Models |
|
Spectrum Analyzer |
N9030B Opt 5xx1 |
N9030A Opt 5xx1 |
|
BNC Cable |
Note: For adjustment accuracy, use short, equal-length cables at the I and Q outputs. |
|
|
|
|
|
|
|
Use the two 6" BNC cables to connect the UUT I and Q outputs to the BNC Tee. |
.
If this adjustment fails, perform the following steps in order:
Check the equipment setup (see above). If the setup is incorrect, make the necessary corrections and rerun the adjustment.
If this adjustment fails with the equipment set up properly, refer to the troubleshooting section of the signal generator's service guide. If you do not have a printed copy of the service guide (Option OBW), one is available either on the CD-ROM that came with your signal generator shipment or on the Keysight Website.
If you cannot correct the problem using the troubleshooting procedures in the Service Guide, obtain service from Keysight Technologies. Refer to Contacting Keysight Technologies.