This adjustment corrects for the differences in the FM source signal paths. During this adjustment, scaling factors are determined for each FM source signal path for a given modulation signal level. The FM deviation is the same and independent of the signal source or the signal path.
This adjustment starts by setting the signal generator to 1 GHz with an FM deviation of 117.1875 kHz. The INT1 path is selected and the modulation level is set to 0 V. The output frequency is measured using a frequency counter and stored. The modulation level is then changed to –2.5 V and the output frequency is measured. The difference between the two frequencies is compared to a target deviation and used to determine a scaling factor. The process for calibrating EXT1 and EXT2 paths and determining the scaling factors is the same except that a function generator is used to provide a modulation level of 1 V and a digital multimeter is used to set the modulation level.
|
Test Equipment |
Recommended Model |
Alternate Model |
|
Frequency Counter |
53230A Opt [106 or 115] |
53132A Opt 010 and [050 or 124] |
|
Function Generator |
33622A |
33611A 33250A |
|
Digital Multimeter |
3458A Opt 002 |
34470A |
|
|
|
Setup 1
Setup 2
Setup 3
If this adjustment fails, perform the following steps in order:
Check the equipment setup (see above). If the setup is incorrect, make the necessary corrections and rerun the adjustment.
If this adjustment fails with the equipment set up properly, refer to the troubleshooting section of the signal generator's service guide. If you do not have a printed copy of the service guide (Option OBW), one is available either on the CD-ROM that came with your signal generator shipment or on the Keysight Website.
If you cannot correct the problem using the troubleshooting procedures in the Service Guide, obtain service from Keysight Technologies. Refer to Contacting Keysight Technologies.