The purpose of this calibration is to optimally set the LBOUT/HBOUT:VBLO_DAC on the output board for use in the digital mode of operation. The LBOUT/HBOUT: VBLO_DAC on the output board is used to control the bias voltage to the internal I/Q modulator mixers. The LBOUT/HBOUT: VBLO_DAC primarily is used to adjust the mixer bias for optimum I/Q modulation linearity (low intermodulation distortion and I/Q modulation errors), but it has a secondary influence on the mixer gain. The goal of this calibration is to have sufficient power through the I/Q modulator to perform the desired modulation (have enough UUT output power available), while minimizing intermodulation distortion when digital modulation is in use.
For frequencies > 4 GHz, default DAC values are used.
|
Test Equipment |
Recommended Model |
|
50 ohm Termination |
909A Opt 012 |
|
|
|
If this adjustment fails, perform the following steps in order:
Check the equipment setup (see above). If the setup is incorrect, make the necessary corrections and rerun the adjustment.
If this adjustment fails with the equipment set up properly, refer to the troubleshooting section of the signal generator's service guide. If you do not have a printed copy of the service guide (Option OBW), one is available either on the CD-ROM that came with your signal generator shipment or on the Keysight Website.
If you cannot correct the problem using the troubleshooting procedures in the Service Guide, obtain service from Keysight Technologies. Refer to Contacting Keysight Technologies.