Adjacent channel power ratio (ACPR) is the ratio of the power level in an adjacent channel (PADJ) to the average power level in the main channel (PMAIN):
ACPR(dBc) = DP = PADJ- PMAIN
In this test, the ESG is configured to generate either an IS–95 CDMA Reverse or FWD 9/FWD 64 modulation pattern in the main channel.
Adjacent-channel power is measured by a spectrum analyzer in a 30 kHz bandwidth at an offset frequency of 885 kHz from the center of the main channel.
|
Test Equipment |
Critical Specifications for This Test |
Recommended Models |
Alternate Models |
|
Spectrum Analyzer |
Noise Floor ≤ –91 dBm |
N9030B Opt 5xx1 |
N9030A Opt 5xx1 |
|
|
|
|
If this performance test fails, perform the following steps in order:
Check the equipment setup (see above). If the setup is incorrect, make the necessary corrections and rerun the performance test.
If this test fails with the equipment set up properly, refer to the troubleshooting section of the signal generator's service guide. If you do not have a printed copy of the service guide (Option OBW), one is available either on the CD-ROM that came with your signal generator shipment or on the Keysight Website.
If you cannot correct the problem using the troubleshooting procedures in the Service Guide, obtain service from Keysight Technologies. Refer to Contacting Keysight Technologies.