|
|
This test requires firmware revision C.05.82 or later. |
This test compares the digital modulation power level to the CW power level at the same frequency. If the UUT is not equipped with an internal digital baseband generator, then its external I/Q inputs are driven by an external baseband generator. A power meter and power sensor are used to measure the UUT output power in CW mode and in digital-modulation mode. The difference between the two power levels is compared to the specifications.
The test is performed with three different modulation formats: QPSK, GMSK, and WCDMA.
|
Test Equipment |
Critical Specifications for This Test |
Recommended Models |
Alternate Models |
|
External Baseband Signal Generator |
Used only if the UUT does not have a Baseband Generator Opt 001, 002, 601, or 602 |
N5182B Option 656 or 657 |
N5182A Opt 651, 652, or 654 E4438C Opt 001, 002, 601, or 602 |
|
Power Sensor |
None |
N8482A |
N8482A CFT |
|
Power Meter |
None |
N1914B |
N1914A2 E4418A |
Option H84 provides reflection coefficient data.
Power meter N1914A with serial numbers ranging between MY00000000—MY53040007 require Service Note 07 to be applied for measurement repeatability. Please have this service note applied or verify it was applied before using this power meter. The affected service note is N1914A-07.
|
|
|
This test uses flexible power sensor channel assignment and will identify the channel that a power sensor is connected to using the ability of "smart" sensors such as the N848xA, U848xA, and E930xA series to report their full model and serial number. Legacy 848x series power sensors are unable to provide their model or serial number, but their channel is identified during the sensor calibration process by identifying the channel of the sensor connected to the calibrator.
If the wrong legacy power sensor is connected to the calibrator during this process the error can be resolved by disconnecting and reconnecting the power sensor to the power meter which will force a new calibration.
If this performance test fails, perform the following steps in order:
Check the equipment setup (see above). If the setup is incorrect, make the necessary corrections and rerun the performance test.
If this test fails with the equipment set up properly, refer to the troubleshooting section of the signal generator's service guide. If you do not have a printed copy of the service guide (Option OBW), one is available either on the CD-ROM that came with your signal generator shipment or on the Keysight Website.
If you cannot correct the problem using the troubleshooting procedures in the Service Guide, obtain service from Keysight Technologies. Refer to Contacting Keysight Technologies.