Power level accuracy is the difference between the power level indicated by the unit under test (UUT) and the true power delivered by the UUT.
Direct absolute power measurements are made with a power meter for higher power levels. A spectrum analyzer is used for all lower power measurements.
|
Test Equipment |
Recommended Models |
Alternate Models |
|
Power Meter |
N1914B |
N1914A1 E4418A |
|
Power Sensor |
N8482A |
E9304A N8482A CFT 8482A2 U8481A Option 200 |
|
Spectrum Analyzer |
N9030B Opt 5xx4, MPB, Pxx5 |
N9030A Opt 5xx4, MPB, Pxx5 E444xA3
Opt 110 and 123 |
Power meter N1914A with serial numbers ranging between MY00000000—MY53040007 require Service Note 07 to be applied for measurement repeatability. Please have this service note applied or verify it was applied before using this power meter. The affected service note is N1914A-07.
Not allowed for the following product configurations:
The dynamic frequency range of this sensor is insufficient for these models.
Depending on your frequency needs, choose either an E4440A, E4443A, E4445A, E4446A, E4447A, or E4448A.
Depending on your frequency needs, choose the option of PXA spectrum analyzer (503, 508, 513, 526, 543, 544, 550) that has a maximum frequency greater than or equal to the maximum frequency of the unit under test.
Select any preamplifier option for the PXA spectrum analyzer (P03, P08, P13, P26, P43, P44, P50) that has a maximum frequency greater than or equal to the maximum frequency of the unit under test.
|
|
|
Connect all test equipment as shown.
Connect GPIB cables to all GPIB-controlled test equipment.
While performing this test, follow all instructions on the controller display.
This test uses flexible power sensor channel assignment and will identify the channel that a power sensor is connected to using the ability of "smart" sensors such as the N848xA, U848xA, and E930xA series to report their full model and serial number. Legacy 848x series power sensors are unable to provide their model or serial number, but their channel is identified during the sensor calibration process by identifying the channel of the sensor connected to the calibrator.
If the wrong legacy power sensor is connected to the calibrator during this process the error can be resolved by disconnecting and reconnecting the power sensor to the power meter which will force a new calibration.
Select from the links below for connection setups depending on the power sensor.
Sometimes noise from nearby test equipment can affect low-level measurements. Errors may be caused even if the power meter is stacked on top of the spectrum analyzer.
Inspect all RF cables. If semi-rigid cables are used, check for cracks in the shielding or at the connectors. RF leakage to/from the cables generally cause problems at higher frequencies (> 2 GHz) and low power levels (< -100 dBm).
Verify that the spectrum analyzer does not have a residual spur at the frequency being measured. Sometimes a spur will limit how low in power the spectrum analyzer can measure.
Make sure that all test equipment is using the same power outlet. Ground loops can cause problems at low power levels. This type of problem will most likely show up at lower frequencies.
Make sure all covers on the DUT are secure and that all screws are in place.
Verify the amplifier being used meets its gain specifications.
Make sure all connections in the measurement system are torqued properly. Loose or damaged connections result in RF leakage and errors result at low power levels.
Make sure all test equipment (including the amplifier) has been
turned on at least 45 minutes.