A dc voltage is used to switch the UUT pulse modulation on and off. A spectrum analyzer is used to measure the power of the fundamental (CW) frequency of the UUT with the pulse on and off. The difference in these power levels is the pulse on/off ratio, in dB.
|
Test Equipment |
Critical Specifications for This Test |
Recommended Models |
Alternate Models |
|
Spectrum Analyzer |
Marker Accuracy |
N9030B Opt 5xx1 |
N9030A Opt 5xx1 E444xA2 Opt 233 |
|
Function Generator |
None |
33622A |
33250A |
|
|
|
|
If this performance test fails, perform the following steps in order:
Check the equipment setup (see above). If the setup is incorrect, make the necessary corrections and rerun the performance test.
If this test fails with the equipment set up properly, refer to the troubleshooting section of the signal generator's service guide. If you do not have a printed copy of the service guide (Option OBW), one is available either on the CD-ROM that came with your signal generator shipment or on the Keysight Website.
If you cannot correct the problem using the troubleshooting procedures in the Service Guide, obtain service from Keysight Technologies. Refer to Contacting Keysight Technologies.