This manual test verifies that the signal generator's single sideband phase noise meets specification. During this test, a phase noise system and a reference source are used to measure the single sideband phase noise of the signal generator. The phase noise is measured at 20 kHz offsets to different test frequencies and compared to specifications.
If a failure occurs, it may not be due to the signal generator. For some test conditions, the signal generator specifications are better than the reference source specifications. If a failure occurs, a three-source comparison should be performed at this carrier frequency to identify a true failure.
|
|
When mapping the Phase Noise Reference Source in TME, the sources you can choose from are prefixed with "PNRS_" (e.g., "PNRS_E8257D"). This prefix is used to distinguish these sources from the sources that must be on the GPIB bus (the Reference Source is not required to be on the bus). If you map the same device as a Reference Source and as something else, you will need to enter the serial number and calibration due date each time because TME treats each mapping as a different device. |
|
Test Equipment |
Recommended Models |
Alternate Models |
|
Phase Noise System |
N5511A Options 540, CH21 |
E5505A |
|
Reference Source2 |
E8257D3 Opt UNR, UNX, or UNY |
8664A Opt 004, |
|
Cable |
8120-4921 APC 3.5 (m) to (m) |
|
|
Cable |
11500C Type-N (m) to (m) |
|
|
Cable |
8120-1840 BNC (m) to (m) |
|
|
Adapter |
E9625A BNC Tee (m) (f) (f) |
|
|
Adapter |
11901D 2.4 mm (f) to APC 3.5 (m) |
|
|
Adapter |
1250-1749 APC 3.5 (f) to (f) |
|
|
|
|
|
There are two sets of procedures depending on the model of the phase noise test system used:
N5511A Phase Noise Test System (PNTS), recommended phase noise test system
E550xA/B, legacy phase noise test systems
Select from the links below according to the phase noise test system being used.
Connect all test equipment as shown.
Connect GPIB cables to all GPIB-controlled test equipment.
Preset all test equipment and the DUT.
Change the following parameters in the N5510A PNTS user interface:
Select the View pull-down menu.
Select Display Preferences and un-check the Spurs box.
Select OK to close Display Preferences.
Select the System pull-down menu and select Server Hardware Connections.
Select or ensure the following:
FFT Analyzer has Keysight M9551A selected.
Select Close to close Server Hardware Connections.
Select the Define
pull-down menu, select Measurement, and select the
following settings:
|
Parameter |
Setting |
||||||||||||||
|
|
|
||||||||||||||
|
Type and Range Tab |
|||||||||||||||
|
Measurement Type |
Absolute phase noise (using a phase locked loop) |
||||||||||||||
|
Measurement Method |
Fast |
||||||||||||||
|
Start Offset Resolution Expansion |
10 |
||||||||||||||
|
Channel Setup |
Single |
||||||||||||||
|
Start Offset Frequency |
0.9 Hz (must be < first specified offset frequency) |
||||||||||||||
|
Stop Offset Frequency |
110 MHz (must be > last specified offset frequency) Limited to:
|
||||||||||||||
|
FFT Analyzer Minimum Number of Trace Averages |
40 |
||||||||||||||
|
RBW % |
7.84 (256 point FFT) |
||||||||||||||
|
FFT Overlap % |
75 |
||||||||||||||
|
FFT Window Type |
Flat Top |
||||||||||||||
|
|
|
||||||||||||||
|
Sources Tab |
|||||||||||||||
|
Carrier Source Frequency |
Obtain tested frequencies from the TME data entry form. |
||||||||||||||
|
Carrier Source Power |
The carrier source power should be set to the power for which the phase noise specification applies. The ESG-C does not specify a power level. Historically it has been tested at +14 dBm up to 1 GHz, and +10 dBm at ≥ 2 GHz. |
||||||||||||||
|
Detector Input Frequency |
Same as Carrier Source Frequency |
||||||||||||||
|
Reference Source Power |
+15 dBm to 3 GHz |
||||||||||||||
|
VCO Nominal Tune Constant |
|
||||||||||||||
|
VCO Tune Range |
|
||||||||||||||
|
VCO Input Resistance |
|
||||||||||||||
|
Center Voltage |
0 |
||||||||||||||
|
|
|
||||||||||||||
|
Cal Tab |
|||||||||||||||
|
Phase Detector Constant |
Derive detector constant from measured beat note |
||||||||||||||
|
VCO Tune Constant |
Measure VCO Tune Constant |
||||||||||||||
|
Verify calculated phase lock loop suppression |
Blank |
||||||||||||||
|
|
|
||||||||||||||
|
Spurious Tab |
|||||||||||||||
|
Mark Spur |
Checked |
||||||||||||||
|
Minimum Limit |
4 dB |
||||||||||||||
|
Maximum Limit |
50 dB |
||||||||||||||
|
|
|
||||||||||||||
|
Block Diagram Tab |
|||||||||||||||
|
Carrier Source |
Manual |
||||||||||||||
|
Reference Source |
Model number of reference source |
||||||||||||||
|
Phase Detector |
Automatic Detector Selection |
||||||||||||||
|
Test Set Tune Voltage Output |
Front Panel |
||||||||||||||
|
Test Set Tune Voltage Destination |
Reference Source |
||||||||||||||
|
VCO Tune Mode |
|
||||||||||||||
|
|
|
||||||||||||||
|
Test Set Tab |
|||||||||||||||
|
LNA Low Pass Filter |
Internal — Selected Auto — Checked |
||||||||||||||
|
LNA Gain |
Auto Gain — Selected Minimum Auto Gain — 14 dB |
||||||||||||||
|
PLL Integrator Attenuation |
0 dB |
||||||||||||||
|
Use Channel #2 |
Unchecked |
||||||||||||||
|
|
|
||||||||||||||
|
Graph Tab |
|||||||||||||||
|
Title |
User specified |
||||||||||||||
|
Graph Type |
Single-sideband phase noise (dBc/Hz) |
||||||||||||||
|
X Scale minimum |
Same as start offset frequency |
||||||||||||||
|
X Scale maximum |
Same as stop offset frequency |
||||||||||||||
|
Y Scale maximum |
0 dBc/Hz |
||||||||||||||
|
Y Scale minimum |
–170 dBc/Hz |
||||||||||||||
|
Normalize Trace Data |
1 Hz bandwidth |
||||||||||||||
|
Trace Smoothing Amount |
0 |
||||||||||||||
Making the Measurement
Set the DUT frequency to the first carrier frequency and power in the TME data entry form.
Set the DUT RF Output to On.
Ensure that the 10 MHz reference of the DUT is set to internal. (The EXT REF annunciator should not be displayed. If it is, check for a signal going to the 10 MHz IN connector.)
If testing a DUT with Option UNX, UNY, or HNY, ensure that the Optimize φ Noise is set to Optimize φ Noise Offset < 150 kHz (Mode 1). To do this, press Frequency > More > MoreOptimize φ Noise and select Optimize φ Noise Offset < 150 kHz (Mode 1).
Select the Measure pull-down menu and select New Measurement.
When the measurement completes, select the Markers icon and place markers at specified offsets to determine the measured phase noise. When specifying a marker offset, the marker will be set to the closest frequency on the graph as indicated in the following table:
|
Nominal Offset |
Actual Offset |
|
1 Hz |
1.0245 Hz |
|
10 Hz |
10.058 Hz |
|
100 Hz |
99.838 Hz |
|
1 kHz |
1.0014 kHz |
|
10 kHz |
9.9182 kHz |
|
20 kHz |
19.836 kHz |
|
100 kHz |
100.71 kHz |
|
1 MHz |
1.001 MHz |
|
10 MHz |
10.059 MHz |
|
100 MHz |
100 MHz |
For carrier frequencies above 3 GHz, the following connection changes are required:
Connect the Reference Source Output to the 1.2 GHz to 40 GHz Ref/LO Input of the M9550A Phase Detector module in the N5511A PNTS.
If a failure occurs, a three-source comparison measurement should be performed at the same carrier frequency to identify a true failure.
Setup with a carrier frequency of 500 MHz
Connect all test equipment as shown.
Connect GPIB cables to all GPIB-controlled test equipment.
Preset all test equipment and the signal generator.
Connect the E8257D RF output to the N5500A reference input.
Connect the N5500A Tune Voltage Output to the E8257D Ext 1 input.
|
Table 1: E4438C and E4428C Carrier Test Frequencies and Power |
||
|
Frequency (MHz) |
DUT Power (dBm) |
Reference Power (dBm) |
|
500 |
14 |
12 |
|
1000 |
14 |
12 |
|
2000 |
10 |
5 |
|
3000 |
10 |
5 |
|
4000 |
10 |
5 |
|
6000 |
10 |
5 |
In the Keysight N5505A Phase Noise System user interface, change the following parameters:
Select the View pull down menu.
Select Display Preferences and clear the Spurs box.
Select OK to close Display Preferences.
From the System pull down menu, select Server Hardware Connections.
Ensure the correct FFT Analyzer is selected, either the 11 PCI20428W-1 or the 89410A.
Connect the signal generator's RF OUTPUT to the N5500A signal input.
Connect the 70420A or N5500A 50 kHz to 1600 MHz Reference Input to the Reference Generator RF Out.
Connect the 70420A or N5500A Tune Voltage Output to either the FM input (8665B) or the Ext 1 (PSG) input of the Reference Source.
From the Define pull down menu, select Measurement, and set the following:
|
Parameter |
Setting |
|
|
|
|
Type and Range Tab |
|
|
Measurement Type |
Absolute phase noise |
|
Start Offset Frequency |
1 Hz |
|
Stop Offset Frequency |
1 MHz |
|
FFT Averages |
4 |
|
FFT Quality |
Normal |
|
Swept Quality |
Normal |
|
|
|
|
Sources Tab |
|
|
Carrier Source Connected |
Test Set |
|
Carrier Source Frequency |
See Table 1. |
|
Carrier Source Power |
See Table 1. |
|
Detector Input Frequency |
See Table 1. |
|
Reference Source Power |
See Table 1. |
|
VCO Tune Constant |
1,000 Hz/Volt |
|
VCO Tune Range |
5 volts for PSG |
|
VCO Input Resistance |
50 ohms for PSG |
|
|
|
|
Cal Tab |
|
|
Measure Phase Detector Constant |
Checkmark |
|
Measure VCO Tune Constant |
Checkmark |
|
Verify calculated phase lock loop suppression |
Blank |
|
Phase Lock Loop Suppression |
Use theoretical value. |
|
|
|
|
Block Diagram Tab |
|
|
Carrier Source |
Manual |
|
Down Converter |
None |
|
Reference Source |
E8257D |
|
Phase Detector Mode |
Automatic |
|
Test Set Tune Voltage Destination |
Reference Source |
|
VCO Tune Mode |
DCFM |
|
|
|
|
Test Set Tab |
|
|
Input Attenuation |
0 dB |
|
LNA Low Pass Filter |
Auto |
|
LNA Gain |
Auto |
|
PLL Integrator Attenuation |
0 dB |
|
|
|
|
Downconverter Tab |
|
|
Input Attenuation |
Auto |
|
IF Gain |
Auto |
|
Microwave/Millimeter Band |
Microwave (0 – 26.5 GHz) |
|
Reference Chain Reference |
10 MHz |
|
External Tune Enable |
Checkmark |
|
|
|
|
Graph Tab |
|
|
Title |
User specific |
|
Graph Type |
Single-sideband phase noise (dBc/Hz) |
|
X Scale minimum |
1 Hz |
|
X Scale maximum |
1E+6 |
|
Y Scale maximum |
0 |
|
Y Scale minimum |
–170 |
|
Normalize Trace Data |
1 Hz bandwidth |
Set the signal generator frequency to the first carrier frequency and power in Table 1.
Set the RF Output to on.
Perform a phase noise measurement.
From the Measure pull down menu, select New Measurement.
Place a marker at 20 kHz offset.
Compare the marker amplitude value to the specifications displayed by the software.
Print out a phase noise plot.
The measurement data must be entered into the following form displayed on-screen when the test is run. The specifications shown below may differ from those displayed by the software based on the internal hardware of the particular DUT.
Enter the measured value from the phase noise system into the "Measured Value" column for the appropriate frequency/offset frequency combination. All values must be entered for the test to complete. Entering a measured value and then clicking in the "Result" column in the form will cause the result to appear.
If the "Guardbanding On" checkbox is not selected, then the result will be of the form PASS/FAIL. Otherwise, the result will be calculated using the displayed uncertainty and will be in the form PASS/FAIL/INDETERMINATE. The specification against which the measured value is compared is displayed in the "< Specifications" column.
If this performance test fails, perform the following steps in order:
Check the equipment setup (see above). If the setup is incorrect, make the necessary corrections and rerun the performance test.
If this test fails with the equipment set up properly, refer to the troubleshooting section of the signal generator's service guide. If you do not have a printed copy of the service guide (Option OBW), one is available either on the CD-ROM that came with your signal generator shipment or on the Keysight Website.
If you cannot correct the problem using the troubleshooting procedures in the Service Guide, obtain service from Keysight Technologies. Refer to Contacting Keysight Technologies.