This adjustment calibrates the FM offset by calling the firmware DCFM cal and storing the result in the cal array.
The firmware DCFM cal is performed by the presto modulation filter. The calibration removes all DC offsets from the modulation-path multiplexer to the ADC. This is done by connecting the input of modulation ADC to the ground (through the modulation-path multiplexer) and then letting the presto modulation filter capture DC offset.
|
Test Equipment |
Recommended Model |
Alternate Model(s) |
|
Spectrum Analyzer |
PXA N9030B Option Pxx1
|
PXA N9030A Option Pxx1 PSA models Option [1DS or 110]1: |
|
|
|
If this adjustment fails, perform the following steps in order:
Check the equipment setup (see above). If the setup is incorrect, make the necessary corrections and rerun the adjustment.
Check for DC offsets after the modulation path multiplexer.
Refer to the troubleshooting section of the service guide. If you do not have a printed copy of the service guide (Option OBW), one is available either on the CD-ROM that came with your signal generator shipment or on the Keysight website.
If necessary, obtain service from Keysight Technologies. Refer to Contacting Keysight Technologies.