|
|
The RF ABUS Calibration must be performed prior to this calibration. |
The goal of this calibration is to determine the tuning sensitivity of the reference oscillator (Kv). This value is used by firmware to control the reference system. This adjustment will set the reference oscillator N.f number and measure its corresponding frequency outputs. The data will be used to calculate the tuning sensitivity of the reference oscillator (Kv).
|
Test Equipment |
Recommended Model |
Alternate Model(s) |
|
Spectrum Analyzer |
PXA N9030B Option Pxx1
|
PXA N9030A Option Pxx1 PSA models Option [1DS or 110]1: |
|
|
|
If this adjustment fails, perform the following steps in order:
Check the equipment setup (see above). If the setup is incorrect, make the necessary corrections and rerun the adjustment.
Refer to the troubleshooting section of the service guide. If you do not have a printed copy of the service guide (Option OBW), one is available either on the CD-ROM that came with your signal generator shipment or on the Keysight website.
If necessary, obtain service from Keysight Technologies. Refer to Contacting Keysight Technologies.