|
|
The RF ABUS Calibration must be performed prior to this adjustment. |
The goal of this calibration is to determine the optimal offset pretune DAC setting for each offset loop frequency. This data is used by firmware to pretune the offset loop system to guarantee that the offset loop locks to the correct frequency. The offset loop is opened and the adjustment is performed using the offset loop under/over indicators to determine the optimal offset loop control DAC setting. The loop is then closed and the integrator voltage is measured to ensure that the loop locked to the correct frequency.
|
Test Equipment |
Recommended Model |
Alternate Model(s) |
|
Spectrum Analyzer |
PXA N9030B Option Pxx1
|
PXA N9030A Option Pxx1 PSA models Option [1DS or 110]1: |
|
|
|
If this adjustment fails, perform the following steps in order:
Check the equipment setup (see above). If the setup is incorrect, make the necessary corrections and rerun the adjustment.
Refer to the troubleshooting section of the service guide. If you do not have a printed copy of the service guide (Option OBW), one is available either on the CD-ROM that came with your signal generator shipment or on the Keysight website.
If necessary, obtain service from Keysight Technologies. Refer to Contacting Keysight Technologies.