Amplitude switching speed is defined as the time required for the DUT to switch from one amplitude to another. Switching starts at the receipt of a SCPI command or trigger signal. Switching ends when the signal amplitude settles to within 0.2 dB.
|
Test Equipment |
Critical Specifications for This Test |
Recommended Model |
Alternate Models |
|
Spectrum Analyzer |
Sweep Time Accuracy |
N9030B Opt 5xx1 |
N9030A Opt 5xx1 |
|
Function Generator |
|
33622A |
33611A |
|
|||
|
|
|
If this performance test fails, perform the following steps in order:
Check the equipment setup (see above). If the setup is incorrect, make the necessary corrections and rerun the performance test.
Refer to the troubleshooting section of the service guide. If you do not have a printed copy of the service guide (Option OBW), one is available either on the CD-ROM that came with your signal generator shipment or search for your signal generator model number on the Keysight website.
If necessary, obtain service from Keysight Technologies. Refer to Contacting Keysight Technologies.