Error Vector Magnitude (EVM) is the magnitude of the vectorial difference between the measured signal and an ideal reference signal in the I-Q plane.
Global Phase Error is the magnitude of the phase difference between the measured signal and an ideal reference signal in the I-Q plane.
This test supports two different test setups using either a PXA (N9030A/B) signal analyzer with Vector Signal Analysis Application, or an 89441 vector spectrum analyzer. The PXA is the preferred solution.
A PXA-series (N9030A/B) signal analyzer is used with the 89600 Vector Signal Analysis Application to measure EVM and Global Phase Error.
A PSA-series spectrum analyzer (E4443A, E4440A, or E4445A) with Option 241 (Flexible Digital Modulation Personality) and B7J (Digital Demodulation Hardware) and Option 123 (Preselector Bypass)4 may also be used to measure EVM and Global Phase Error.
|
Test Equipment |
Critical Specifications for This Test |
Recommended Model |
Alternate Models |
|
Signal Analyzer |
EVM Accuracy |
N9030B Opt 5xx1 and MPB2 |
N9030A Opt 5xx1 and MPB2 |
|
Vector Signal Analysis Application5 |
|
896006, 7 VSA with these options:
|
|
|
|||
An 89441A vector spectrum analyzer is used to measure EVM and Global Phase Error. When using the 89441A, additional equipment is required for downconverting the signal above 2.65 GHz.
|
Test Equipment |
Critical Specifications for This Test |
Recommended Model |
Alternate Models |
|
Vector Signal Analyzer |
EVM Accuracy |
89441A Opt AYA, AYH, AY9, B7A, and UFG or UTH |
|
|
Mixer |
Frequency Range: |
0955-2225 |
0955-1017 |
|
Local Oscillator |
Output power1:
≥ 16 dBm |
E8257D Opt [UNR or UNX or UNY] |
E8241A Opt UNJ |
|
10 dB Attenuator |
None |
8491B Opt 010 |
8490D Opt 010 |
|
|||
|
|
|
click here.
click here:When adding the PXA as LAN device, use the PXA's Hostname rather than the IP Address to avoid the possibility of crashing the software. The Hostname can be found in the PXA's System menu. An example of a Hostname is: K-N9030B-80323, where K = Keysight, N9030B = model, 80323 = last 5 digits of the serial number.
If the VSA software freezes during the Digital Modulation Quality test, manually verify that the you are able to “Rediscover Instruments” in the VSA software.
Next, click on the Discover Instruments tab and click on the Rediscover Instruments button.
If this freezes, then you may need to set the Keysight VISA as the Preferred VISA. To set the Keysight VISA as the preferred VISA:
Open the Keysight Connection Expert and go to Settings > Visa Conflict Manager > General VISA Settings. Ensure Keysight VISA is set as the preferred VISA implementation as shown in the image below: