This test verifies that the internal pulse modulator's rise and fall time meets specifications.
Pulse modulation rise/fall time is defined as the amount of time it takes the pulse envelope to transition from the 10% pulse envelope level to the 90% pulse envelope level on both the rising and falling edges of the pulse.
During the test, the signal generator is placed in an internal pulse modulation mode at a certain power level and the rise and fall time of the pulse envelope is measured with a high-frequency, digitizing oscilloscope.
|
Test Equipment
|
Recommended Model |
Alternate Model(s) |
|
High Frequency Oscilloscope Mainframe |
N1000A |
86100A/B/C/D |
|
Oscilloscope Plug-In |
N1045B1 |
N1045A1 83484A 86112A |
|
10 dB Attenuator |
8493C Opt 010 |
8490D
Opt 010 |
|
20 dB Attenuator |
8493A
Opt 020 |
8490D
Opt 020 |
|
|
|
click here:
If this performance test fails, perform the following steps in order:
Check the equipment setup (see above). If the setup is incorrect, make the necessary corrections and rerun the performance test.
Refer to the troubleshooting section of the service guide. If you do not have a printed copy of the service guide (Option OBW), one is available either on the CD-ROM that came with your signal generator shipment or search for your signal generator model number on the Keysight website.
If necessary, obtain service from Keysight Technologies. Refer to Contacting Keysight Technologies.