AM distortion is defined as the square root of the ratio of the power contained in the harmonics of the demodulated AM waveform to the power of the fundamental component of the demodulated waveform.
This is essentially a total harmonic distortion (THD) measurement, and is made directly by the audio analyzer. The THD indicated by the audio analyzer includes the distortion added by the measuring receiver.
|
Instrument |
Critical Specifications for This Test |
Recommended Model1 |
|---|---|---|
|
Measuring Receiver |
AM Demodulated Distortion (<50% AM) ≤ 0.3% |
8902A |
|
Audio Analyzer |
Distortion (20 Hz to 20 kHz) < –80 dB2 |
8903B |
|
Mixer3 |
RF/LO Freq.
Range: 1 to 2800 MHz |
M/A-COM MDC-164 |
|
Local Oscillator3 |
Frequency Range: 800 to 2500 MHz Amplitude:16 dBm |
E8267D |
|
|
|
|
Measuring Receiver Calibration Setup
AM Distortion CW Frequency < = 1300 MHz Test Setup
AM Distortion CW Frequency > 1300 MHz