FM frequency responseverifies that a selected FM deviation remains constant within ±1 dB as the FM rate is varied from 80 Hz to 100 kHz and the DUT CW frequency is varied from 500 MHz to 1.0 GHz. If the DUT meets the frequency response specification in this CW frequency range, frequency response in all other frequency ranges will be assured.
FM deviation is set to 100 kHz at an FM rate of 1 kHz. The actual deviation is measured with a measuring receiver and stored as the reference deviation. While the deviation setting remains at 100 kHz, actual deviation is measured for FM rates between 80 Hz and 100 kHz. If the measured deviation at any test rate is more than 1 dB different from the reference deviation at 1 kHz, the test fails. Each frequency is tested with this sequence:
A reference signal is measured.
The set deviation is measured for each applied rate change.
Each deviation measurement is compared to the reference deviation.
The comparison is a calculation of the difference in the deviations relative to the reference rate. The relative value is the FM frequency response.
|
Instrument |
Critical Specifications for This Test |
Recommended Model1 |
|---|---|---|
|
Spectrum Analyzer |
FM Deviation Accuracy |
E444xA2 Opt 1DS, 1233 |
|
Function Generator |
33250A |
|
|
Digital Voltmeter |
3458A Opt 002 |
|
|
|
|
Measuring Receiver Calibration Setup
FM Frequency Response Test Setup