FM deviation accuracyis checked for CW frequencies from 500 MHz to 1.0 GHz. If the DUT meets the accuracy specification in this frequency range, accuracy in all other frequency ranges will be assured.
A measuring receiver is used to demodulate the FM signal and indicate the recovered FM deviation. The measuring receiver is calibrated prior to the measurement.
|
Instrument |
Critical Specifications for This Test |
Recommended Model1 |
|---|---|---|
|
Spectrum Analyzer |
FM Deviation Accuracy |
E444xA2 Opt 1DS, 1233 |
|
Function Generator |
none |
33250A |
|
Digital Voltmeter |
AC True-RMS Accuracy |
3458A Opt 002 |
|
|
|
|
Measuring Receiver Calibration Setup
FM Deviation Accuracy Test Setup