This adjustment characterizes the RF chain with baseband 1 GHz band scanning through the full RF frequency with the limited RF spacing from 19.5 GHZ to 44 GHz.
Test Equipment |
Recommended Model Number |
Alternate Model Number |
---|---|---|
Power meter |
N1914B |
N1913B N1914A1 N1912A E4419A2 |
Power sensor 1 |
N8488A |
None |
|
|
Channel 2 setups apply only to signal generators with Option 002 which adds a second channel. Channel 2 tests/adjustments will be run after all Channel 1 tests/adjustments have been run. |
This test/adjustment uses flexible power sensor channel assignment and will identify the channel that a power sensor is connected to using the ability of "smart" sensors such as the N848xA and U848xA series to report their full model and serial number.